AXIS#.VL.KVFF

Description

This parameter sets the gain for the velocity feedforward (a scaled derivative of the position command is added to the velocity command value). The nominal feedforward value can be multiplied by this gain value.

This parameter is only used in the position mode (AXIS#.OPMODE = 2).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

NA

Range

0 to 2

Default Value

1

Data Type

Float
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
AXIS1.VL.KVFF

5011h

04h

Signed32

-

1000:1

Read/Write

No

AXIS2.VL.KVFF

5111h

04h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.KVFF

6030

178E

Signed32

Read/Write

-

AXIS2.VL.KVFF

71566

1178

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.KVFF

6030

Float

Read/Write

-